Prints a selected set of content.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overloads MustOverride Sub Print( _
ByVal results As IList(Of View) _
) |
Parameters
- results
- A list of View objects to print. The list of all printable views can be retrieved using the Display.Views property. Note that you can print either individual results (traces, marker window, output window, etc.) or full windows (the main window or any trace windows), but not a mixture of the two. Any attempt to mix individual results and windows in a single call will lead to an System.ArgumentException being generated.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also